This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561:Seeking assistance with programming Golden Image via I2C for BQ27Z561

Part Number: BQ27Z561
Other Parts Discussed in Thread: BQSTUDIO, EV2400

Tool/software:

I developed a battery gauge using BQ27Z561 and created a golden image.

In order to mass-produce after development, I will manufacture electrical circuit boards equipped with BQ27Z561, but I am having trouble writing the golden image from the host MCU via the I2C I/F.

My questions are

- Are there any apps or subprograms for writing the golden image from the host MCU via the I2C I/F? #Something that runs on Linux is OK.

This is something that runs on Linux.

As this involves modifying the electrical circuit board, the option of connecting an external device such as EV2400 and writing with bqStudio is not available, so it has been excluded.

Thank you in advance.