Other Parts Discussed in Thread: TPS548C26, , LMR36503, LMR36510
Tool/software:
Hi team,
My customer is asking about do we have such spec like other device listed? Looks like only DC spec shown.
TPS548C26
LMR36503-Q1
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
My customer is asking about do we have such spec like other device listed? Looks like only DC spec shown.
TPS548C26
LMR36503-Q1
Hi Oliver,
The spec in the LMR36503 refers to DC as well. We have a spec for the LMR36510, which maintains the similar maximum voltage, but the minimum value is -3.5V. However, we cannot guarantee the sub-10ns transient for the LMR36503 as we did not spec it in the datasheet.
Thanks,
Richard
Hi Richard,
If we have not spec of the sub-10ns, could you please help check below attached waveforms looks fine or not? To me, these looks fine to me.
Vin is 54V, Vout is 3.3V, peak load is 0.3A.
We would like to make sure the overshoot and undershoot is within spec, thank you.
Full load_max
Full load_min
Light load_min
Light load_max