This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR38020: Incorrect switching frequency

Part Number: LMR38020

Tool/software:

Hi, 

We are using the LMR38020FSDDAR (fixed PWM, spread spectrum variant) to step a rail down from 24V to 5V. We are using the RT_SYNC pin with an external resistor 52.3kR to set the switching frequency to 500kHz. However, when measuring the ripple, we can see that the regulator is operating at 2MHz. This is happening with multiple boards and we're unsure why the switching frequency is wrong. Can you advise what might cause this?

Many thanks