Other Parts Discussed in Thread: LM3409
Tool/software:
Hi TI Team,
I am currently in need of an LED driver that can meet specific requirements. The driver should be capable of delivering a maximum output exceeding 1.0A and support low-level analog dimming (0~10%).
The application I’m working on requires a 1 Amp LED driver that offers analog dimming and emits low noise, as it is intended for use in medical equipment. The driver should be capable of operating 4 LEDs simultaneously.
At present, I am utilizing the LM3409 demo board. However, I am encountering issues with output ripple and an inability to achieve zero current with analog dimming.
I am wondering if anyone has encountered similar issues and found solutions to these problems.
Ultimately, my goal is to find a driver that can provide an output ranging from 0 to 1A. If anyone has recommendations for a suitable IC or any technical documentation that could assist me, I would greatly appreciate it.
Please note that I intend to implement analog dimming using a potentiometer.