Other Parts Discussed in Thread: TPS709, TLV760
Tool/software:
Hi,
We want to choose a LDO for the power supplier, and our paramater is input voltage is 24V, and output voltage/current is 5V/100mA, the package is SOT23-3;
We consider to use the TLV709 but we can't find the pad on the bottow of this package, we are affraided the temperature rise because the power dissipation is more than 1.9W,
We calculate the temperature based on below thermal information form, the temperature rise is very high and it is unacceptable,
so please kindly advise if there are any other LDO that it has the PAD for the heat dissipation? thanks.