This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Can BQ76952 identify disconnection faults?

Prodigy 220 points
Part Number: BQ76952

Tool/software:

If my AFE is not connected to the battery cell and the temperature NTC, at this time, if the overvoltage fault, undervoltage fault, overtemperature protection, and undertemperature protection are correctly configured and enabled, will the above faults be reported instead of correctly identifying the disconnection situation?

For example, if a battery cell is not connected, the undervoltage protection is triggered, but it cannot be recognized as a disconnection.