Tool/software:
Hi,
We have a device that is powered by a LiFePO4 battery. The device uses a modem, which means that we need 3.8V. Therefore, we decided to use a step-up from Vbat to 5V, and step-downs for the MCU (3.3V) and modem. The modem block is disconnected during these tests.


We are facing an issue of a large current pulse caused by MCU consumption change. It happens when the MCU is returning from Standby mode -> consumption on 3.3V rises from 0.5-2 µA to hundreds of mA. This causes an extreme current peak on Vbat, which is "un-welding" the cables from the battery.
What can we do?
Thanks in advance,
Vladislav