Other Parts Discussed in Thread: UCC256404
Tool/software:
Hi TI team
Greetings!
We are planning to use 400V to 12V LLC converter using UCC256404 IC.
In order to have tight CTR tolerance wrt ageing we have planned to use optoemulator ISOM8110DFGR.
In this optoemulator if i allow If = 5mA then my CTR variation is narrowed to only between 100% to 155%.
But in that case UCC256404 FB pin could source only maximum of 85uA. In that case how do i use the optoemulator ?
If forward current of 5mA is not possible then for atleast 2mA of forward current how do i design my FB pin of UCC256404.
Also if i bias FB pin externally using RVCC will it disturb the feedback information of UCC256404 ( iam sourcing externally instead of pulling current from FB pin)
Please advice in this regard.
Regards
Rahamadullah