Tool/software:
Hello.
I would like to confirm the Vocth of the OC pin.
Vocth (Detection Threshold) is specified as follows on the data sheet.
Vcoth min 0.63V - max 0.77V
However, when I measured at -20C, it was 0.61-0.63V, which is outside the specifications.
Could you tell me the rason why it is outside the spec.