Other Parts Discussed in Thread: BQSTUDIO
Tool/software:
Hi, TI team.
If I do not have a product board (sense resistor 20mΩ) with Gauge on it, can I proceed with the development using the following procedure?
If there are any errors or improvements in this procedure, could you please point them out?
1. Configure with EVM (sense resistor 10mΩ), set ChemID and DF, learning cycle, extract golden image
2. Change DF value CC Gain manually (from 10mΩ to 20mΩ) according to the specification of the product board
3. Extract Golden image (CC Gain was changed, so it was extracted again)
This is an idea to facilitate several developments at the same time. After completion of the product board, formal CC Offset related calibration will be performed on the product board.