Other Parts Discussed in Thread: LMV358
Tool/software:
Hi Team,
Could you please provide Storage humidity and operating humidity for the below mentioned parts:
UCC27525DR
LMV358IDRG4
LM3480IM3-5.0/NOPB
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Aravind,
The storage humidity is the MSL rating, which can be found under the "Ordering & quality" section on the device's product page. The MSL rating for the UCC27525DR is Level-1-260C-UNLIM, which is the highest rating and considered as being not moisture sensitive even at 85% relative humidity. Devices with a level 1 rating do not require dry packaging. More information can be found in this app note: https://www.ti.com/lit/an/spraby1a/spraby1a.pdf
The operating humidity is usually not stated as the operating performance of most ICs are not dependent on humidity. If humidity is a factor in performance, then it will be specified in the datasheet (humidity sensor is an example).
The other two devices are part of different product lines, so I will be handing this thread over to the team owning the LMV358.
Thanks,
Rubas
Hi Aravind,
Please see the moisture sensitivity search on ti.com: https://www.ti.com/packaging/docs/mslsearch.tsp
The LMV358 is a MSL-Level 1 and can reference the same app note as above. If you have specific questions about the other devices, please start a new thread specifically for the individual devices with those questions or let us know in this thread.
Thank you!
Regards,
Ashley