Other Parts Discussed in Thread: BQ40Z50, EV2400
Tool/software:
Hi,
When I first connected the BQ40Z50 IC to BQStudio via the EV2400 module all of the data was pulled up.
However, I adjusted the CC1 and CC0 bit values within the Data Memory - DA Configuration page and now BQStudio does not recognize the IC. I may have shut off both bit 1 (CC1) and bit 0 (CC0). Is it possible that I mistakenly directed the IC to not recognize the battery cells which in turn has shut off power to the IC?
Is there anything I can do to resolve this and get the IC to be recognized again?
Best regards,
Joe DeWitt