This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561: bq27z561 learning cycle question

Part Number: BQ27Z561
Other Parts Discussed in Thread: BQSTUDIO

Tool/software:

Hello,

Was performing a learning cycle and reached calculated cutoff current for the datasheet.  I never saw the Batterys status flag get set while charging. Am I supposed to just let the battery keep charging endlessly until getting the flag?

Currently relaxing the battery-Hoping that FC flag gets set.

Charging was performed with power supply CC/CV.  4.2V taper current was selected as 300mA. 

battery used was inr18650-35e rated at 3400mAh. 

Discharge was down to 2.66V

standard charge for the battery is 4.2V with 68mA cutoff and 1700mA.  Our pack is 4p arrangement so I used 68mA*4 = 272mA for pack cutoff, pack as charged at 4A CC, 4.2V

-Craig