Other Parts Discussed in Thread: GPCCHEM
Tool/software:
Hi,
I was charging my pack when i noticed the RSOC went from 72%~100% in a small amount of time
this is a little bit strange
See screenshot:

Logs which shows the jump from 72% to 100%:
Wed Jul 17 13:58:16 BST 2024 Device Version Info = 4500_2_11 BQZ Device Name = bq40z50R2 BQZ Firmware Version = V2_11_BLD52 Design Capacity = 3200 Design Voltage = 12800 Specification Info = 0x0031 Manufacturer Date = 2023-10-14 Serial Number = 0x00AE Manufacturer Name = FUJI Device Name = 7250064S2P Device Chemistry = LIFE Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,MaxTurboPwr,SusTurboPwr,MaxTurboCurr,SusTurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,vBAT,vPACK,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellPower1,CellPower2,CellPower3,CellPower4,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,GaugeTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,NoLoadRemCap,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,CompRes1,CompRes2,CompRes3,CompRes4,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,QMax1,QMax2,QMax3,QMax4,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,RawDOD_2,RawDOD_3,RawDOD_4,CBTime1,CBTime2,CBTime3,CBTime4,CBDOD_1,CBDOD_2,CBDOD_3,CBDOD_4,CBTotalDODChg,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus 1,2024-07-17 13:58:20,4.006,0x0387,300,10,0x6001,0,65535,65535,1,25.0,14150,789,287,1,72,87,2765,3852,65535,65535,163,900,14000,0x0080,4,-10188,-7567,-9096,-6400,100,0x0387,0x0002,0x08,0x0008,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3458,3604,3496,3621,14177,14177,754,754,754,754,261,272,264,273,1079,448,25.8,25.0,24.7,196.5,196.4,25.0,24.7,25.0,2766,3554,3852,4984,3220,3071,3953,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,3,3203,3203,3203,3203,-2,-2,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-2,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1319,SUCCESS 2,2024-07-17 13:58:24,8.014,0x0387,300,10,0x6001,0,65535,65535,1,25.0,14254,439,374,1,72,87,2766,3852,65535,65535,128,900,14000,0x0080,4,-10188,-7567,-9096,-6400,100,0x0387,0x0002,0x08,0x0008,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3456,3641,3504,3654,14250,14253,358,354,349,344,124,129,122,126,535,528,26.0,25.0,24.7,196.3,197.9,25.0,24.7,25.0,2767,3555,3852,4984,3220,3071,3953,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,7,3203,3203,3203,3203,-2,-2,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-2,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1217,SUCCESS 3,2024-07-17 13:58:28,12.025,0x0387,300,10,0x6001,0,65535,65535,1,25.0,14265,182,345,1,72,87,2767,3852,65535,65535,138,900,14000,0x0080,4,-10188,-7567,-9096,-6400,100,0x0387,0x0000,0x08,0x0008,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3450,3652,3500,3663,14258,14259,170,168,166,164,59,61,58,60,241,488,26.2,25.0,24.7,196.4,196.4,25.0,24.7,25.0,2767,3555,3852,4984,3220,3071,3953,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,11,3203,3203,3203,3203,-2,-2,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-2,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1170,SUCCESS 4,2024-07-17 13:58:32,16.032,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14270,113,294,1,72,87,2767,3852,65535,65535,159,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0000,0x08,0x0008,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3448,3656,3497,3667,14259,14260,104,106,102,100,36,39,36,37,154,417,26.3,25.0,24.7,197.4,196.4,25.0,24.7,25.0,2767,3556,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,15,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1351,SUCCESS 5,2024-07-17 13:58:36,20.034,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14267,84,246,1,72,87,2767,3852,65535,65535,190,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0000,0x08,0x0008,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3446,3658,3494,3669,14261,14263,82,80,75,75,28,29,26,28,114,349,26.4,25.1,24.7,196.4,196.3,25.1,24.7,25.1,2767,3556,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,19,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1240,SUCCESS 6,2024-07-17 13:58:40,24.045,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14267,69,205,1,72,87,2767,3852,65535,65535,228,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0000,0x08,0x0008,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3445,3659,3493,3671,14261,14261,70,71,70,66,24,26,24,24,96,290,26.6,25.1,24.7,196.5,196.5,25.1,24.7,25.1,2767,3556,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,23,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1373,SUCCESS 7,2024-07-17 13:58:44,28.060,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14268,59,171,1,72,87,2767,3852,65535,65535,273,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0000,0x08,0x0008,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3444,3661,3492,3672,14260,14266,61,61,58,54,21,22,20,20,83,242,26.5,25.1,24.7,196.4,196.5,25.1,24.7,25.1,2767,3556,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,27,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1247,SUCCESS 8,2024-07-17 13:58:48,32.062,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14269,53,143,1,72,87,2767,3852,65535,65535,327,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0000,0x08,0x0008,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3445,3662,3491,3673,14262,14264,54,55,55,49,19,20,19,18,76,203,26.6,25.1,24.7,196.5,195.3,25.1,24.7,25.1,2767,3556,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,30,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1170,SUCCESS 9,2024-07-17 13:58:52,36.074,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14269,44,120,1,72,87,2768,3852,65535,65535,390,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0000,0x08,0x0008,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3445,3662,3490,3674,14263,14263,48,46,42,40,17,17,15,15,66,170,26.6,25.1,24.7,196.4,196.4,25.1,24.7,25.1,2768,3556,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,34,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1234,SUCCESS 10,2024-07-17 13:58:56,40.081,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14269,46,102,1,72,87,2768,3852,65535,65535,458,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0000,0x08,0x0008,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3444,3663,3489,3674,14262,14267,48,46,43,37,17,17,15,14,61,145,26.7,25.1,24.7,196.5,196.5,25.1,24.7,25.1,2768,3556,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,39,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1398,SUCCESS 11,2024-07-17 13:59:00,44.092,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14269,40,87,1,73,88,2795,3852,65535,65535,537,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0000,0x08,0x0808,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3443,3663,3489,3675,14267,14269,39,36,37,35,13,13,13,13,54,124,26.7,25.1,24.7,196.1,196.4,25.1,24.7,25.1,2822,3627,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,43,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1373,SUCCESS 12,2024-07-17 13:59:04,48.102,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14270,40,75,1,76,91,2904,3852,65535,65535,623,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0000,0x08,0x0808,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3444,3663,3488,3676,14269,14263,34,34,37,33,12,12,13,12,50,107,26.8,25.1,24.7,196.5,196.7,25.1,24.7,25.1,2931,3770,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,46,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1234,SUCCESS 13,2024-07-17 13:59:08,52.114,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14270,34,65,1,79,95,3012,3852,65535,65535,719,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0000,0x08,0x0808,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3444,3664,3488,3675,14266,14264,37,37,37,33,13,14,13,12,49,93,26.9,25.1,24.7,197.0,196.4,25.1,24.7,25.1,3039,3913,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,50,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1300,SUCCESS 14,2024-07-17 13:59:12,56.129,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14270,36,58,1,81,98,3120,3852,65535,65535,806,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0000,0x08,0x0808,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3443,3664,3488,3676,14263,14269,35,37,38,35,12,14,13,13,53,82,26.8,25.1,24.7,196.4,196.3,25.1,24.7,25.1,3148,4056,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,54,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1352,SUCCESS 15,2024-07-17 13:59:16,60.139,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14270,27,51,1,84,101,3229,3852,65535,65535,916,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0002,0x08,0x0808,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3444,3664,3488,3676,14268,14268,30,27,28,26,10,10,10,10,39,73,27.0,25.1,24.7,196.4,196.7,25.1,24.7,25.1,3256,4199,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,58,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1293,SUCCESS 16,2024-07-17 13:59:20,64.151,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14270,28,47,1,86,104,3310,3852,65535,65535,994,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0002,0x08,0x0808,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3445,3665,3487,3676,14267,14266,27,31,23,18,9,11,8,7,37,65,27.0,25.1,24.7,196.5,196.5,25.1,24.7,25.1,3364,4342,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,62,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1122,SUCCESS 17,2024-07-17 13:59:24,68.157,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14269,29,42,1,89,107,3419,3852,65535,65535,1140,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0002,0x08,0x0808,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3443,3664,3487,3676,14266,14270,28,28,32,25,10,10,11,9,39,59,27.0,25.1,24.7,196.4,196.4,25.1,24.7,25.1,3473,4485,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,66,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1448,SUCCESS 18,2024-07-17 13:59:28,72.161,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14269,24,39,1,92,111,3527,3852,65535,65535,1198,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0002,0x08,0x0808,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3443,3664,3487,3676,14266,14269,30,27,29,24,10,10,10,9,36,54,27.0,25.1,24.7,196.4,196.4,25.1,24.7,25.1,3581,4627,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,70,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1347,SUCCESS 19,2024-07-17 13:59:32,76.170,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14271,30,36,1,95,114,3635,3852,65535,65535,1298,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0002,0x08,0x0808,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3445,3666,3487,3677,14270,14268,30,30,31,24,10,11,11,9,43,50,27.1,25.1,24.7,196.5,195.6,25.1,24.7,25.1,3690,4770,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,74,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1136,SUCCESS 20,2024-07-17 13:59:36,80.183,0x0387,300,10,0x6001,0,65535,65535,1,25.1,14270,22,34,1,98,117,3744,3852,65535,65535,1375,900,14000,0x0080,4,-10362,-7583,-9252,-6400,100,0x0387,0x0002,0x08,0x0808,0x10,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3445,3665,3487,3677,14267,14269,26,24,22,18,9,9,8,7,31,47,27.0,25.1,24.7,195.0,196.1,25.1,24.7,25.1,3798,4913,3852,4984,3221,3072,3954,782,1032,3851,4983,25.0,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,78,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1234,SUCCESS 21,2024-07-17 13:59:40,84.190,0x4383,300,10,0x6001,0,65535,65535,1,25.1,14268,4,31,1,100,121,3851,3851,65535,65535,1508,0,0,0x40A0,4,-10362,-7583,-9252,-6400,100,0x4383,0x0002,0x08,0x00C8,0x1A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3443,3663,3486,3675,14263,14269,0,0,0,0,0,0,0,0,0,0,27.2,25.1,24.7,196.4,196.4,25.1,24.7,25.1,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,0,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1349,SUCCESS 22,2024-07-17 13:59:44,88.198,0x4383,300,10,0x6001,0,65535,65535,1,25.1,14261,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10362,-7583,-9252,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3444,3661,3485,3673,14254,14265,0,0,0,0,0,0,0,0,0,0,27.0,25.1,24.7,196.3,196.5,25.1,24.7,25.1,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,4,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1137,SUCCESS 23,2024-07-17 13:59:48,92.209,0x4383,300,10,0x6001,0,65535,65535,1,25.1,14256,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3443,3658,3485,3671,14247,14265,0,0,0,0,0,0,0,0,0,0,27.0,25.2,24.7,196.5,195.6,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,8,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1296,SUCCESS 24,2024-07-17 13:59:52,96.210,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14251,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3443,3656,3484,3669,14243,14265,0,0,0,0,0,0,0,0,0,0,27.0,25.2,24.7,195.9,196.4,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,12,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1139,SUCCESS 25,2024-07-17 13:59:56,100.223,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14246,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3443,3654,3484,3667,14237,14265,-1,-4,-2,-9,0,-1,-1,-3,-4,0,27.0,25.2,24.7,196.4,196.3,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,16,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1332,SUCCESS 26,2024-07-17 14:00:00,104.230,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14242,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3652,3483,3665,14233,14266,0,0,0,0,0,0,0,0,0,-1,27.0,25.2,24.7,196.4,196.4,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,20,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1120,SUCCESS 27,2024-07-17 14:00:04,108.240,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14237,0,-1,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3650,3483,3663,14230,14264,0,0,0,0,0,0,0,0,0,-1,26.9,25.2,24.7,196.4,196.5,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,24,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1191,SUCCESS 28,2024-07-17 14:00:08,112.254,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14233,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3442,3648,3482,3661,14224,14265,0,0,0,0,0,0,0,0,0,-1,27.0,25.2,24.7,196.5,196.4,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,28,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1335,SUCCESS 29,2024-07-17 14:00:12,116.261,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14229,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3440,3646,3482,3660,14223,14264,0,0,0,0,0,0,0,0,0,0,27.0,25.2,24.7,196.4,196.4,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,32,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1248,SUCCESS 30,2024-07-17 14:00:16,120.271,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14226,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3442,3645,3482,3658,14218,14263,0,0,0,0,0,0,0,0,0,0,27.0,25.2,24.7,196.4,196.4,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,36,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1361,SUCCESS 31,2024-07-17 14:00:20,124.284,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14223,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3440,3643,3482,3656,14215,14265,0,0,0,0,0,0,0,0,0,0,27.0,25.2,24.7,196.5,196.4,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,40,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1238,SUCCESS 32,2024-07-17 14:00:24,128.293,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14221,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3440,3642,3482,3655,14212,14264,0,0,0,0,0,0,0,0,0,0,27.0,25.2,24.7,196.5,195.6,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,44,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1244,SUCCESS 33,2024-07-17 14:00:28,132.305,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14217,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3440,3640,3481,3653,14208,14265,0,0,0,0,0,0,0,0,0,0,27.0,25.2,24.7,196.5,196.5,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,48,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1278,SUCCESS 34,2024-07-17 14:00:32,136.317,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14214,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3440,3638,3481,3652,14205,14265,0,0,0,0,0,0,0,0,0,0,27.0,25.2,24.7,194.9,196.4,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,52,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1238,SUCCESS 35,2024-07-17 14:00:36,140.327,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14211,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3440,3637,3481,3651,14203,14266,0,0,0,0,0,0,0,0,0,0,27.0,25.2,24.7,196.5,195.9,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,56,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1305,SUCCESS 36,2024-07-17 14:00:40,144.342,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14208,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3440,3636,3481,3649,14200,14266,0,0,0,0,0,0,0,0,0,0,27.1,25.2,24.7,196.0,196.5,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,60,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1323,SUCCESS 37,2024-07-17 14:00:44,148.346,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14205,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3440,3634,3481,3648,14197,14265,0,0,0,0,0,0,0,0,0,0,27.1,25.2,24.7,196.1,196.4,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,64,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1221,SUCCESS 38,2024-07-17 14:00:48,152.358,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14202,-3,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3440,3633,3481,3647,14194,14265,0,0,0,0,0,0,0,0,0,-1,27.1,25.2,24.7,196.4,195.3,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,68,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1200,SUCCESS 39,2024-07-17 14:00:52,156.371,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14200,0,0,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3440,3631,3481,3646,14192,14265,0,0,0,0,0,0,0,0,0,0,27.1,25.2,24.7,195.7,196.3,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,72,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1104,SUCCESS 40,2024-07-17 14:00:56,160.379,0x4383,300,10,0x6001,0,65535,65535,1,25.2,14197,0,-1,1,100,121,3851,3851,65535,65535,65535,0,0,0x00E0,4,-10382,-7586,-9270,-6400,100,0x4383,0x0000,0x08,0x00C8,0x5A,0x1018,0x01B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3440,3631,3481,3644,14189,14266,0,0,0,0,0,0,0,0,0,-1,27.1,25.2,24.7,196.4,196.1,25.2,24.7,25.2,3851,4983,3851,4983,3221,3851,4983,782,1032,3851,4983,25.1,25.0,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,76,3203,3203,3203,3203,-3,-3,1,0,0,0,0,4000,4000,4000,4000,3203,3203,3203,3203,-3,1,2.46,1233,8,8,8,8,0,0,0,0,8,8,8,8,16384,3818,4951,1473,SUCCESS
Regards
Jonathan Kabangu