Other Parts Discussed in Thread: BQSTUDIO
Tool/software:
Good Day .
We are testing the SCD on our high current system ( 16 s / 300A )
Shunt is a 300 A 75 mV . Normal current measurement and all other functions of the BMC chip are working fine .
For testing basic SCD action we set the trip level to " 0 " 10 mV over the shunt value . We expect the SCD to be detected once we pass 10mV -
We ramp up the current by selecting loads , 4mV - all good 8mV all good 12 mV SCD trip - and if we remove the load it will reset itself after about 5 sec . NO problem .
We can ramp the current up to increase the shunt voltage well above 10 mV and it works fine (the trip action ) - but only on one board of 3 battery packs that are connected in parallel .
3 identical battery packs - each with its own bms unit and shunt . Only the one bms chip /board will detect the set SCD limit and react on it .
All 3 have the exact same settings programed , same circuit . Even when we test the battery packs on their own - 2 of the 3 will not react to a SCD limit event .
We unplugged all cables to the pcb - total power cycle , verified the set values in the BMS chip ( write to an read out of BMS chip to verify ) but no improvement.
Chip is not in TEST mode .
Any idea why 2 out of 3 will not work as expected ?
Kind regards
Nico