Tool/software:
Dear TI
i verify web bench for ucc28070 below condition
Vac: 190~265
Vout: 390V
Iout: 9V
custum freq: 30kHz
other condition : dithering + best eff
20220129_제니스_TI_PFC_재검토_20220615_WBDesign230.pdf
20240710_MPP_TI_PFC_UCC28070_WBDesign281.pdf
i find some different value of parts(maybe five parts)
and most value of different parts is similar.(Cpv Ccdr Cpbc, Cpca)
but Cfa, Cfb is very different. 220nF(2022) > 220pF(2024)
L3,L3 inductance is so different. 220uH(2022) > 174uH(2024) ( it is not possible to control custum inductance)
i have two question.
First Question different value of parts, Cfa Cfb is so different, why? which do i choice value?
Second Question, PFC inductance, how do i tune for custom inductance of web bench?
Best regards, Choi