Tool/software:
Hello,
I want to be able to disable the TLV70033 output using the switch S1 as shown below, so that a user can connect an external voltage up to 5.5V instead of the regulated 3.3V. Would it be ok to apply 5.5V on the OUT pin like this? The recommended operating conditions for VOUT is 4.8V max, but the abs max is 6V so I think it would be fine. Thanks!
Best,
Sakeenah Khan