This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5810: Behavior when VCC and VLD are different

Guru 12175 points
Part Number: LP5810

Tool/software:

Hi,

I am considering the following circuit configuration.
・VMCU=VCC=3.3V
・VLED=5V

Q1. Will it break if VCC=OFF, VLED=5V temporarily? In the above case, the LED lights up, and it seems that about 3V is applied from VCC via VLED→LED→OUT.

Q2. Can it be used with VCC=3.3V, VLED=5V? Can it be used even if the voltage of VCC and VLED are not the same? As far as I can see from the data sheet, VCC and VLED are defined separately.

Thanks,

Conor