This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25628: Looking for Battery Charger for Coin Cell

Part Number: BQ25628

Tool/software:

May I know we have solution to support BR2032 Lithium Fluorocarbon Button Batteries.

https://www.omnergybattery.com/product/br2032-lithium-fluorocarbon-button-batteries

Specifications
Nominal Discharge current 0.2mA
Nominal Voltage 3V
Nominal Capacity 200(mAh)
Continuous stangard load 15(kΩ)
Maximum pluse current 6mA
Operating temperature -40℃~85℃
Weight 3.0(g)
UL Recognition MH29853

BR,

Gary