This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25750: Reverse mode operation and current limit

Part Number: BQ25750


Tool/software:

HI,

What i understand the reverse mode of BQ25750, is operating buck-boost path reversely without VAC and only connected battery.

Also BQ25750 monitor and regulates the battery discharging current and it can control by register setting.

Q1) If the battery discharging current touch the limit, does it stop to buck-boost switching immediately?

Q2) At this time Q1, How does it operate BATFET ? because reverse mode turns off BATFET already, but the system still needs to source power.

Q3) Generally, I expect to battery discharging current(System load) is more higher than buck-boost converting output load. IBAT_REV register can be setted 20A, How can I control(design) if system load is more higher?

Thanks.