Tool/software:
Hi,
I have a solar cell with MPP = 4.5V, 40mA and VOC = 5.6V. I want to harvest power from it at maximum power point and run a 100ohm load at 3V as the energy is available from the solar cell. There is no need to use a battery in my design and I want to just use a 100uF capacitor instead of battery.
Can BQ25570 be used for such application and what is the efficiency I can get from it in such scenario?