Other Parts Discussed in Thread: LM5155
Tool/software:
Hello, I am trying to simulate custom schematic of a LM3488 Boost converter. On device page there are two simulation files: encrypted and unencrypted. I downloaded Orcad free trial and watched some tutorials how to perform transient analysis. I am still very new to Orcad and only know the basic functions, but I managed to import .OPJ file of a encrypted version, and Inside there are two simulations prepared, but as I said, I need to create my custom schematic with different values and a bit different component placement. I tried using model of this file on my simulation project and I got error after running simulation:
Here is the schematic of my simulation project
I don't really know what is the problem, because I just added encrypted file library and inserted LM3488 component on my schematic. I tried using unencrypted file, but it only has .lib file, which I tried adding and then using a bit differently looking LM3488 symbol, but got same error.


Can someone please help me and give a step by step tutorial how to import just a symbol of LM3488 file into OrCad and how to use it to simulate circuit that I showed above? Or maybe how to fix current error and simulate transients?


Is it even possible to use my chips model for custom designs ? Because as I understand, it provides start-up and some other simulation, you can select it by setting SS to 0 or 1. Does it work like regular spice model ? Can I use it to simulate output voltage, current, power, calculate efficiency? Because my goal is to see how my circuit behaves on certain scenarios, loads and get output voltage, output current, efficiency coefficient, also output voltage ripple and compare them with different components.