Tool/software:
Hello Guang,
You mentioned "the default value of internal DEVADDR[3] for TPS929240A-Q1 is set to 1 and can be used with TPS929240-Q1 to achieve maximum 16 devices on one FlexWire bus; Also due to it, register CRC value is different."
I have one more question: If customer can set DEVADDR[3] bit to 1 in TPS929240-Q1 register manually? so that customer do not need to purchase different OPN devices.
Thanks!