Other Parts Discussed in Thread: TLV62130, , TPS62903
Tool/software:
Hi, Ti power management team
Can i replace the TLV62130 in the following two scenarios:
Application
-
MCU Power
- Voltage / Current : 3.3V / 100mA
-
BATTERY Input Source
- Voltage / Current : 5V / 3A
Questions
1) For the TPS563206, the SW pin is connected to the BTST pin via a Via. Will this have a negative impact on EMI?
2) Is it acceptable to connect the SW pin with a thin trace?
3) Are there any precautions to take?
Regards.
Jeong.