Tool/software:
Hi Team,
We are planning to use TPS4H160-Q1 for a four-channel lighting load, the load current requirement is 2.5+0.5+0.5+0.3=3.8A. We calculated the thermal with 85C, each channel overcurrent capacity is 1.3A, looks good overall.
While we found in the datasheet, nominal DC load current is marked as 0-2.5A. Is this 2.5A means the current on each channel cannot exceed 2.5A? I suppose the overcurrent limit is configurable which is 8A. Are I understand the correct?
We concern the requirement for each channel is 2.5A, peak current is below 5A, while the constant current might exceed 2.5A a little bit. Would that be a problem?
Thanks
Best,
Frank