Tool/software:
HI,
Can you please provide the minimum / typical / maximum startup time under the following conditions?
- Input voltage will rise to 2.5V at rate of 10mV / us
- Output voltage will be 1.8V
- Expected current draw will be 100mA
- 1uF capacitor on output pin
- Enable pin will be tied to input voltage
The startup time(s) we are looking for is from input voltage = 0V to output voltage = 1.8V with the criteria specified above.
Thanks.