This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: BQ25756 VAC_DPM_STAT

Part Number: BQ25756

Tool/software:

Dear Support.

I am using a BQ25756.

Charging does not start despite Power Good and CE='L'.

At that time, VAC_DPM_STAT=1.

What is the status of this?

The Power Good range is 40~60V, and charging does not start when the input voltage is 42V or lower.

What could be the problem?

Can you please help me?

Thank you in advance.