A customer is using the TPS23753 PoE controller in an IP-webcam application. They would like to use an op-amp fomr something on the high-voltage (24-60V) side of the converter, and they are wondering if the Vc pin of the TPS23753 can supply the power for it.
The datasheet says the pin is a bias voltage for the DC/DC converter, but it also appears to play a part in startup timing. They would need 10mA from this pin.
I do not expect this to be feasible, but I wanted to run it by the experts first. I will likely just suggest they use an op-amp with high-voltage capability, or to consider using the op-amp on the low-voltage side of the converter.
Thanks!