Tool/software:
Hi,
I am using the TPS23523 in a design to protect the DC input from -37VDC to -60VDC with nominal -48VDC.
Design data are attached in the excel file.
TPS2352X_Excel_Tool_Web_RevB_prueba4.xlsx
Adittionally, I am using the pins Neg48 and Bgate with two 2 N-channel mosfet in parallel (IPB110N20N3LF).
For gate pin, it is used N-channel MOSFET (IPB110N20N3LF) and for gate2 pin theCSD19535KTT.
I have checked the signal in the output of TPS23523 in the starting sequence when 3 different DC power signal of -37VDC, -48VDC and -60VDC are connected to the input of TPS23523.
Please, find attached the different figures.
a) Waveform for 37VDC

b) Waveform for -48VDC

c) Waveform for -60VDC

In these figures, it is observed a different waveform fdepending on the input voltage value and a waveform is repeated several times (3 iterations for -37VDC, 4 iterations for -48VDC and 5 iterations for -60VDC)
Which is the cause of this repeated waveform? It seems that "something" is not right and the sequence is repeated. .
Please, could you indicate us if this repeated waveform is "typical"? If this repeated waveform are not "usual", please. how can I solve it?
Thanks in advance.
Best Regards,
Pedro