This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61040: Design Update failure on Webench Power designer

Part Number: TPS61040
Other Parts Discussed in Thread: TLV61046A, TLV61048

Tool/software:

Hi,

I'm planning to use TPS61040DBVR for below requirement

VIn= 4.8V

Vout=7V

Iout=100 mA

But webench power designer is not allowing me to change the current more than 70mA. It is showing erros as design failed to updated even though TPS61040DBVR supports Vout upto 28V & 400 mA .