This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5026: Vin 48V to Vout 12V(120W) circuit design.

Part Number: LM5026
Other Parts Discussed in Thread: PMP22075, , TL431

Tool/software:

Hello,

I modified the circuit design of LM5026 based on PMP22075, but found that Pulse transformer (T6) makes noise when powered on.

The following are the specifications of the circuit design and schematic, could you help to check what happen in this curcuit?

- Vin = 48V
- Vout = 12V
- Pout = 120W

Isolated power design 48V to 12V (120 Watts).pdf

Pulse transformer PA0937NL

T6_PA0937NL.pdf

Best regards,