Other Parts Discussed in Thread: TPS61099, TPS61299
Tool/software:
We tried to boost the voltage up to 3.5 V from 1.2 V. But the voltage is not increasing . Please help us with its circuit diagram.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
there are only fixed output voltage selection for TPS61322 family device.
See device comparison table in the datasheet.
There is 3.6V output voltage could you accept that. Or you could try TPS61299 or TPS61099 which have more optional output voltage.
What do you mean you can't connect battery at the input? just solder the power in with the Vin pin.