Tool/software:
Hi All
- The output capacitor table for LMR38010 is shown above. For calculations involving a voltage conversion from 24V to 12 V at a frequency of 1000kHz , with an output current of 1A, a current ripple ration of 0.4(dI/Io), calculated inductance value is around 15uH, the minimum capacitance value for a load current change of 0.8 A and a voltage ripple of 3% approximately , calculated value of capacitance is around 1.11 uF, However the table indicates use of two 10uF capacitors. If the derated capacitance of a 10uF capacitor at 12 V and across all temperatures exceed the calculated capacitance of 1.11uF is a single capacitor sufficient ? How do we determine the no of capacitors needed in parallel ?
Formula used to calculate the minimum capacitance required is taken from TI app note SLVA477B
Thanks
Alphons