This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28750: Feedback pin configuration without optocoupler

Part Number: UCC28750


Tool/software:

Hello team,

We are planning to use ucc28750 for multiple output power supply design, so can we use simple resistive voltage divider at FB pin instead of using opto-coupler? We can compromise with isolation. Please share reference also.

  • Hi abhishek

    Thank you for reaching out.

    Yes a simple resistive divider can be used.

    I would prefer something using an arrange shown below with a current feedback which will work with the internal pull up resistor of FB pin.

    Currently there are no reference designs with UCC28750 showing this. But the above concept should work.

    Regards,

    Harish