This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Can you please say me what will be the voltage across the capacitor that connected between CP1 and CP2.
Hi Divyaa,
If Vin is lower than 3V, the internal charge pump works. CP1 will switch between 0 to Vin, and CP2 between Vin to 2Vin.
If Vin is higher than 3V, the internal charge pump is inactive. CP1 is 0 and CP2 is the same with Vin.
If available, could you share the detailed application that the TPS61093 will be used? Thank you.
Regards
Lei