Other Parts Discussed in Thread: BQSTUDIO, , EV2400, USB2ANY, BQ25713
Tool/software:
Hi,
My name is Antonio López, and I have many questions to know if this product is suitable for my project.
- I know that I can monitoring the temperature, battery voltage, and current with the ADC. Can I monitoring these data in real time? If not, which is the period of time to do it?
- Can I program it with a specific voltage an current with the I2C protocol to charge the battery ? For example 4.2 V 8A or 3.8 V 4A.
- Do you recommend before make my own PCB buy the EVM model to test it?
- I know that there's a program to see the registers and programe the IC (BQSTUDIO) but can I use an micrcontroller to comunicate with the BQ?
- I have the symbol and the footprint, but not the model to do a simulation, is it possible to simulate in a specific software?I'm using Proteus.
Best regard,
Antonio