This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62812-Q1: WEBENCH Designer Tool Issue

Part Number: TPS62812-Q1


Tool/software:

Hi,

I want to calculate the TPS62812-Q1 IC power dissipation with following condition.

Vin: 5.499V (min) to 5.843V (max)

Vout: 1.39V

Iout: 0.69A

Ambient Temp: 105°C

Comp Setting: Comp setting 1 with RCF resistor

Mode Setting: FPWM

Soft start time: 4.8 ms

User preferred frequency: 2.2 Mhz (Rcf = 8.2k)

Input capacitance: 6.09 uF x 3 = 18.27 uF
Input capacitors equivalent maximum ESR: 3.6714 mOhms

Inductance: 0.465 uH
Maximum DC resistance: 27 mOhms

Feed forward cap (Cff): 22pF

Rfbt: 27k

Rfbb: 20.5k

Output capacitance: 9.85 uF x 4 = 39.4 uF
Output capacitors equivalent maximum ESR: 2.7528mOhms

I tried to simulate this with WEBENCH tool, but I could not able to modify the values of individual components as per my requirement. When I try to change the value of one component, the values of other components also changes to initial values. Is this a tool related issue or am I missing anything? please help.