This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79656EVM-021: Current Sense in Cell Simulation Mode

Part Number: BQ79656EVM-021


Tool/software:

Hi guys,

I am using the BQ79656EVM-021 with simulated cells and i have an external power source connected to VSTACK and GND.

Now I am trying to measure a current via the voltage on SRP/SRN Pins. I have an external shunt resistor with 4-Terminal-connection in my circuit. The two inner Pins of the shunt are connected to SRP / SRN. I read the Main Current High an Low register but i am only getting my external supply voltage as a result. Even if nothing is connected to SRP/SRN i read the supply voltage of the board from the register.

How can i read the actual voltage on PIN SRN/SRP?

Greetings

Florian