This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2973: Issue recovering from fault mode

Part Number: BQ2973

Tool/software:

Hi, I'm seeing some strange behaviour with the BQ29737 circuit. I'm using it with a single cell battery, no pack, connected directly to a charger as below(charger connected between Vbatt and GND). To test it I have been pulling the battery + and - rails above 4.3V and below 2.8V to confirm the OVP and UVP functionality, and while it kicks in and the FETs turn off at these expected set points, when I set the voltage back to within the normal region (say 3.5 - 4V) it doesn't recover. Interestingly, it only recovers when I either (a) short the cell- net to the system ground net (in the bottom right below) or (b) turn the charger on, then even after toggling the charger back off, the BQ has resolved it's fault. Any ideas? Does the circuit below look reasonable?

Many Thanks,

Dave