Tool/software:
Hi
I use a TPS62841DLC in one of my designs to switch and output a 1.5V from 3.3V input. But for some reason, when I enable the regulator the output seems to be at ~2.6 - 3.3V ( and there seems to be a direct short between Vout and Vin pins when the regulator is enabled). I have verified my boards for any direct short between the pins (post soldering) and there seems to be none and the EN receives a 3.3V (same as that of the input Vin). I have tried to follow the webench designer and datasheet specifications as closely as possible, but I not able to debug as to why this is happening. I have attached the schematic and layout here. I would appreciate any help or suggestion.
I also have a TPS2841 eval board (with a DGR package), and the same settings provides a 1.5V in the eval board.
TPS62841DLCR debug.pdf