Tool/software:
Hi Britton,
I attached the schematic and the filled-out design calculator for your review as we discussed.
I did my best to fill out the schematic checklist on the second page of the design calculator.
I have a few outstanding items that aren't marked closed, particularly for the RSP/RSN pins.
Also, could you recommend a 2.2nF high frequency cap. 0603 25V rated for the switching ripple filtering on VIN. Currently I have a 10nF 16v. At 14V VIN that's probably pretty useless. The datasheet for the TSP543C20 referenced2.2nF high frequency caps at 25V, but I wasn't able to find a PN.
I also placed the snubber circuit at the output as a place holder and DNI'd the components.
In the attachment I have provided an Altium project with the SMPS schematic labeled Switcher B (It is the only completed circuit in the project)
All relevant data sheets are also included in the attachment.
Thanks again for all of your help,
Matt