This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50: FC Flag don't set high on charging terminated /completed ROSC 100%

Part Number: BQ40Z50

Tool/software:

On charging complete FC flag don't set to high charging is completed and ROSC 100%.   I attached configuration file also

FC_ISSUE_18-07-24.gg.csv

  • Hello Moeez,

    Your gg file suggests that the SOC Flag Config B register wasn't configured to set the FC flag when RSOC is 100%. 

    Notice that the register highlighted above shows 0x8c, which is 10001100 in binary. You would need to set FCSETRSOC bit in order for the FC bit to be set.

    Regards,

    Siddharth