Other Parts Discussed in Thread: TLV752
Tool/software:
Dear experts,
We're currently looking into the mentioned part and were wondering if it would be possible to use the PMID output for an integrated class D amplifier instead of for example a phone.
If I understand correctly, we can make the OTG pin high and set the OTG_CONFIG bit through I2C to disable and enable the output on PMID. What can I expect with regards to noise on the PMID output, and how is SW output affected (if it is at all)?
The SW output will be connected directly to a TLV752 which in turn will provide the entire system with 3.3V. It's important that this 3.3V is always stable and low enough noise for an IMU and ESP32. The PMID output may fluctuate a bit, but must not result in distorted audio produced by the MAX98357.
This will work right?
Best regards,
Jochem