This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS274C65EVM: Firmware for use w/ Arduino Uno

Part Number: TPS274C65EVM
Other Parts Discussed in Thread: TPS274C65, TPS274C65USBEVM

Tool/software:

Hi - 

Note from customer: 

I was wondering if you guys could help me with some firmware support for the TI TPS274C65 chip I could run with an Arduino Uno I’m currently using.

I’m looking for something in C/C++/C# that will just allow me to control the switch.  The current sense features on the chip seem really interesting, if that is included on the firmware that would be nice to have.

Is there example code we can use here? Customer wants HW GPIO control to control the HSS - but EVM is only SPI-controlled. 

Note that software links on EVM webpage are broken. 

Thanks,

Tyler