Other Parts Discussed in Thread: UCC256404, UCC256402, TLV431
Tool/software:
Hi TI team
In UCC25640EVM-020 VO618A optocoupler is used.
As per the design the opto LED current is (12V-1.2V)/9.09Kohm = 1.18mA. The CTR of VO618A is 50% to 600% as per the datasheet.
Which will give collector current of 0.594mA to 7.12mA. But as per the datasheet of UCC256404 it says FB pin can source only 85uA maximum. where does the remaining current will be sourced from .
Please clarify if my understanding is wrong.
Regards
Rahamadullah