Tool/software:
We are trying to improve a design with the requirement of creating a high-voltage source (50V) from a lipo-battery (Vin 3 to 5V), with the possibility of sourcing up to 10mA from the high-voltage source.
The current design is based on an LT8570 in boost configuration with a very large inductor, operating in a low-efficiency area.
I'm looking for some alternative solutions that are more efficient and with a smaller footprint. I stumbled on the TPS61391, which may be a reasonable choice, but it comes with extra features (APD and current mirrors), which (I assume) we would not need. I also do not really understand what is the purpose of the APD and if it's necessary since it's referenced in the application
- Can somebody help me understand if this part is adequate for our use case? I'm also looking for alternative solutions (charge pumps maybe?), any suggestion is appreciated!
- What's the point of the APD? Can the converter be used without it?
Thank you!