Other Parts Discussed in Thread: BQ34Z100, BQSTUDIO, EV2400, GPCCHEM
Tool/software:
Hello,
I am trying to complete a learning cycle for a battery pack consisting of 6, 550 mAh, AAA NiMH batteries connected in series on the BQ34Z100 EVM.
I am not seeing the Update Status bit go from 0x4 to 0x5 during the learning cycle.
I have made several attempts, following the instructions in SLUA925 ("How to Complete a Successful Learning Cycle for the bq34z100") and the TRM, chapter 11. I have attached the BQStudio logs from my most recent attempt. This attempt was made by following the 'alternative method' from SLUA925, where IT_ENABLE is sent after the first Discharge->Relax(>5 hours).
I am using dV/dt charge termination, and the FC seems to set at the appropriate time.
I am using CHEMID 6116, as suggested by the GPCHEM tool.
These are the steps from my most recent attempt:
- Program firmware 'bq34z100_v2_02_build_31.srec' to reset IT from most recent attempt.
- Program CHEMID = 6116
- Import all Data Memory Settings (.gg file attached), Set 'Update Status' to 0 (.gg file saved it as x4)
- Calibrate EVM so that Voltage/Current look appropriate
- Completely discharge battery, and let relax overnight for 17 hours
- Issue IT_ENABLE, begin charging @125 mA. Charging circuit is a constant current at 125 mA.
- Wait for [FC] bit to go high. Looks like it was set at the appropriate time (-dV/dt)
- Relaxed overnight for 10 hours
- Discharge with a 100 mA programmable load until 5.4V is seen (900 mV * 6 batteries). (~ 5 hours)
- Relaxed for 5.5 hours ([REST] seen). Update status still reads as 0x4. I also see SOC change from 0% to 7% by end of relaxation cycle. No charger is connected. Not sure why.
- Because of failed attempt, I do another another 'charge, relax, discharge, relax' cycle. Status still reads 0x4
- Firmware Version : bq34z100_v2_02_build_31
- BQStudio Version : 1.3.101 (EV2400)
- dV/dt termination : seems to be working. I see FC set when I'd expect it
I have attached my BQStudio Logs and the .gg file with my register settings. I had to relaunch BQStudio twice, so the logs are split into 3 files, but they are sequential.
Is there something that I am missing here?
Thank you for your help.