Part Number: UC3842
Tool/software:
Hi TI,
How to calculate Css and Rss for soft start in UC3842?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
COMP pin effective range is from 1V to 4.5V. Then, soft start time can be considered from Css = 0.5V to Css = 3.8V.
Considering to approximation of a linear charge, if soft start time tss = 1ms, and if you select Rss = 10k, then
Css = tss x (Vref/Rss) / (3.8V-0.5V)
= 0.001 s x (5V/10k) / 3.3V) = 1.51 x 10^-7 F = 0.151 uF, or 0.15uF
As the real charge is in exponential, so the time would be slightly longer. But the above is good enough to have an initial set of parameters. Then you can do some tuning during bench test.
,