This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92200: Need to know the current consumption on the DIM oin

Part Number: TPS92200
Other Parts Discussed in Thread: TPS92201

Tool/software:

HI Team,

Iam using TPS92200D2DDCR and scheme is shown below

Iam driving the DIM pin of the TPS92200 direcltly by my processor GPIO. And i need to know the current consumption on this DIM pin

  • Hi Deljo,

    This information is not available in the datasheet. I need some time to check this information for TPS92200.

    Meanwhile, I would mention that for 5V input voltage application, TPS92201 is recommended.

    Please let me know if you will keep the design with TPS92200 or if you will change the design to TPS92201. If you will keep the design with TPS92200, then I will check the internal database to see if we have the leakage current data of the DIM pin. If you will change the design to TPS92201, then the leakage current information of the control pins (DIM pin and EN pin) is already available in the datasheet.

    Best Regards,

    Steven