Other Parts Discussed in Thread: TPS923655DMTREVM
Tool/software:
Hi Sir,
Could you share the PWM dimming duty accuracy when TPS923652 is working at the below conditions?
VIN= 5 V, VLED=12V, ILED=100mA.
PWM frequency=10kHz, PWM duty cycle at 3~100%.
PWM signal voltage level: 3.3V(H), 0V(L).
Could you share the PCBA size info(W*L*H) for TPS923655DMTREVM?